Pairing the Device
To pair the device:
- Open Wiser app on your phone.
- On the
Home page (A), tap
Devices (B).
- Tap
(C) to add a device.
- The Add Device page includes the
following tabs:
-
Preferred (D): This tab allows you to select a device directly from the preferred list.
-
Select Preferred > 3Ph Energy Monitoring Device (F).
-
-
All (E): This tab includes all available devices for you to select from.
-
Select All > Energy Meters & Protection> 3Ph Energy Monitoring Device (F).
-
-
- Read the instructions and tap Next.
- Enable permissions to Bluetooth and Wi-Fi for scanning the devices and tap Next.
- Add the following device information and tap Next:
-
Type of location (G): Select the location of the device from drop-down list.
NOTE: If you want to add a custom name of the location, select Enter custom name and enter name in Location Name field. -
Area of the location (in sq ft) (H): Enter the size of the area.
-
Select Room (J): Select the room from drop-down list.
NOTE: If you want to add a custom name of the room, select Add New Room and enter name in Enter Room Name field. -
Name your Energy Meter (K): Enter the device name.
-
Energy Source (L): Select the energy source from drop-down list.
Based on Energy Source selected, you will get additional field to update as shown in following table:
Energy Source Selected
Additional Fields to Update
Grid
Grid Monthly Budget (kWh)
Solar
-
Solar Rated Output in kW
-
Capital Investment
Genset
-
Genset Rating in kW
-
Genset Rating in kVA
-
Power factor rating between 0.1 and 1
-
Voltage Capacity in Volts
-
Current Capacity in Ampere
-
Installation Date
Battery
Battery Capacity in kWh
Electric Vehicle (EV)
Electric Vehicle (EV) Capacity in kWh
Load
-
MCB Connected Room Name
-
Add Connected Load
-
-
- Tap
arrows to read all the instructions under Hardware Installation. Check the following boxes to confirm the status of the LED indicators:
-
Power LED in solid red.
-
Internet LED in blinking red.
NOTE:-
If the Power LED is not in solid red, then check the power connection.
-
If the Internet LED remains in solid red, then tap the reset button four times.
-
If the Internet remains in slow blinking red, then tap the reset button fourteen times.
-
- Tap
to start the Bluetooth scanning.
- Select the Energy Meter device from the list (M).
- Enter the Wi-Fi password and tap Connect (P).
- Now, your Energy Meter is added successfully in the App. You can see the newly added device on the Devices page.