DUG_Energy Monitoring Device Three Phase-01

Voltage and Current Alerts

Set your voltage limits and current limits to get notified during abnormal current fluctuation.
  1. Tap Settings > Voltage and Current Alerts.
  2. Drag the slider button to set the Voltage Lower Limit (A), Voltage Upper Limit (B), and Current limit (C).
  3. To enable Push Notifications, tap button (D).
  4. Follow the same process for the Phase 2 and Phase 3 respectively.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?