DUG_Energy Monitoring Device Three Phase-01

Power Factor Alerts

Get notified when the power factor is below the set value.
  1. Tap Settings > Power Factor Alerts.
  2. Tap to enter Power cut-off value (A).
  3. Tap Push Notifications (B) to enable notifications for Total Power Factor.
  4. Tap Push Notifications (C) to enable phase-wise notifications.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?