DUG_Energy Monitoring Device Three Phase-01

Budgeting

Budgeting allows you to set your budget on daily, weekly, and monthly power consumptions and create alert once you reach certain percentage of that budget.
  1. Tap Settings > Budgeting.
  2. Tap Set budget (A).
  3. Tap against each month field to update monthly budget (B) in kWh.
  4. Tap Save (C) > OK.
  5. Drag the slider button to set the Alert 1 (D) and Alert 2 (E) for monthly budget.
    NOTE: Alert 1 value should always be less then Alert 2 value.
    NOTE: Weekly Budget (G) and Daily Budget (H) are calculated pro rata based on Monthly Budget.
  6. To enable Push Notifications, tap (F) button.
    The app will send you notification of alerts.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?