DUG_Energy Monitoring Device Three Phase-01

Changing the Wi-Fi Access Point

You can change the Wi-Fi network using the Wiser app.
  1. Tap Settings (A) > 3 Ph EMD (B) > Details (C).
  2. Based on device status, take following steps:
    Device Status Steps

    If Device Status is Online.

    1. Tap Change Wi-Fi (D) to change the Wi-Fi network.

      A pop-up will appear, asking for password of Wiser app.

    2. Enter the Wiser app password and tap Confirm.

    3. Select your preferred Wi-Fi network and enter the password in Wi-Fi Password field and tap Connect.

    .

    If Device Status is Offline.

    1. Tap Change Wi-Fi (D) to change the Wi-Fi network.

      A pop up will appear, asking for password of Wiser app.

    2. Enter the Wiser app password and tap Confirm. This will initiate the device pairing mode.

    3. Refer to

      Pairing the Device for the pairing instructions.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?