DUG_Energy Monitoring Device Three Phase-01

LED Indications

Pairing

User Action

LED Indication (Network LED)

Status

Press the reset button 4 times.

Blinking red rapidly.

Pairing mode is active.

Press the reset-button 8 times to change the Wi-Fi access point mode.

Blinking red rapidly.

The device is ready to connect with the new Wi-Fi access point.

NOTE: If there is no CT (Current Transformer) connected to the load, then the LED will not turn ON in the Energy Monitoring Device.

Resetting

User Action

LED Indication (Network LED)

Status

Press the push-button 14 times in 10 s.

Solid red.

The device is in reset mode. It is reset to the factory settings. The device then restarts and the LED stays in red for 10 s before turning off.

Other Indicator Mode

LED Indicator Mode

LED Indication (Channel LED)

Always Off

No LED

Always On

Solid blue

LED Indicator Mode

LED Indication (Network LED)

Reset state, not paired, not added

Solid red

Device paired but not connected to Wi-Fi

Blinking red with 1 second delay

OTA update

Blinking Red and Blue Alternatively

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?