DUG_Energy Monitoring Device Three Phase-01

Energy Tarrif

To effectively use the device you can add the energy tariff information.
  1. Tap Settings > Energy Tarrif.
  2. Select the month (A) you want to update the tarrif.
  3. Tap to add the details (B).
  4. Enter the details in Contracted Load (kW) (C). and Monthly minimum energy charges in ₹ (D).
  5. Select the Energy Tariff Type from the drop-down list.
    • When you select Flat Rate (E), enter the details in Cost per Unit (G).
    • When you select Slab Rate (F), tap Add Slab Rate (H) to add the details.
  6. Tap Save (J).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?