DUG_Energy Monitoring Device Three Phase-01

Live Meter Readings

Get live energy and power reading details from Live Meter Readings.
  1. Tap Settings > Live Meter Readings.
  2. Get following live reading details:
    • Total Imported Energy so far (A)

    • Total Exported Energy so far (B)

    • Total Power now (C)

    • Total Power Factor (D)

    • Average Frequency (E)

  3. Tap Phase 1, Phase 2, and Phase 3 tabs (F) to get the live details phase-wise.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?