DUG_Energy Monitoring Device Three Phase-01

Power Alerts

You can create Power Alerts to get notified on time.
  1. Tap Settings > Power Alerts.
  2. Select any of the Alerts (A) to update following fields (B):
    • Alert Name: Tap to add the name of alert.

    • When: Select Greater Than or Less Than from the drop-down list.

    • Select Value: Tap to add the value.

    • Units

      : Select the unit from drop-down list.
  3. Tap toggle switch (C) to enable the alert.
  4. Tap Save (D) to save the alert.
    NOTE: You can set maximum of eight alerts for each phase.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?