DUG_Energy Monitoring Device Three Phase-01

Updating Firmware

You can update the Wiser app to the latest firmware version.
  1. Tap Settings (A) > 3 Ph EMD (B) > Details (C).
  2. Tap Update Firmware (D).
    A pop up will appear, asking for Wiser app password.
  3. Enter the Wiser app password and Tap Continue.
    An OTP will be sent to your registered email address.
  4. Enter the OTP and tap Submit.
    It will check for the latest version of firmware and update the app.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?