DUG_Energy Monitoring Device Three Phase-01

Managing the Device to Favourites

You can add devices to the favourites list using the Wiser app.
  1. On the Home tab (A), tap next to Your Favourites (B).
    The Edit Favourites page appears.
  2. Tap the star (C) next to the device name.
    The star turns green .
  3. Tap Save (D) to mark the product as favourite.
  4. To remove the device from the favourites:
    1. Tap next to Your Favourites.
    2. Tap the green star to deselect the device and tap Save (D).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?