Add New Tab

This tool allows you to add an additional map display tab. You can have multiple stored displays available on separate tabs. Once you've created a map display tab, select a stored display from the ArcFM Viewer toolbar.

  1. From the File menu, click Add New Tab.

  2. Select a stored display to populate the new map display tab with data.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?