ArcFM Viewer for ArcGIS Engine

ArcFM Viewer, based on Esri's ArcGIS Engine, provides a high-performance, robust query and display tool. With ArcFM Viewer, utility personnel can view, trace, and query data to help minimize cost or optimize the investment in maintenance and construction to get the most from the facility network.

Because ArcFM Viewer is run independent of ArcMap, it may not be opened through ArcMap (like ArcFM). Instead, select ArcFM Viewer for ArcGIS Engine from the ArcFM Solution folder on the Start Menu.

IMPORTANT: If your data was configured for Feeder Manager 2.0 only, you can view it in ArcFM Viewer for ArcGIS Engine. You cannot, however, edit feeder data in mobile sessions. If you do so, the ArcFM Viewer display does not reflect your changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.