Next Upstream Protective Device Trace and Isolation Protective Device Trace

The following table describes the labels applied to protective device features traced by both of these trace tasks. Downstream symbols do not appear in the Next Upstream Protective Device Trace.

Symbol

Meaning

Upstream, closed device

Previously found, upstream, closed device

Downstream, closed device

Previously found, downstream, closed device

Downstream, open device

Previously found, downstream, open device

Indeterminate symbols: Based on the starting point of the trace, it is unknown whether the device is upstream, downstream, energized or de-energized.

Indeterminate, closed device

Previously found, indeterminate, closed device

Indeterminate, open device

Previously found, indeterminate, open device

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?