Login

The Login screen allows the user to select a geodatabase. If you're working with a Mobile application such as Redliner, you'll most likely choose a backdrop database.

Select a database from the drop-down menu, enter a user name and password, and click OK. A password is not required for an Access database.

If you have ArcFM Viewer for ArcGIS Engine installed, values may be added to the drop-down menu using the ArcFM Engine Administrator.

  

Database Mismatch

The database version must match the application version. If you attempt to log in with mismatched versions, you receive the following message:

If you click OK, Engine Viewer opens as usual, but functionality is not supported with mismatched versions. Contact your GIS administrator if you receive the message above.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?