Stored Displays

A utility geodatabase can contain 50 or more feature classes, each of which is represented as a layer in an ArcMap document. Users have a number of standard views or displays, a display being a distinct combination of map layers and layer rendering properties. Individually changing properties of each of the 50 layers to configure a new display could be tedious and error-prone.

Users can access various stored displays by selecting from the Stored Display menu. Use the Add New Tab tool to add another map display tab and select another stored display. ArcFM Viewer does not provide the capability to create or delete stored displays.

If a user happens to select a stored display that has been deleted using ArcFM, that user is notified with a message indicating that the stored display has been removed. The stored display is removed from the list and the user may make a different selection.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.