Electric Trace Tasks
The ArcFM Electric Traces toolbar allows you select the trace you want to perform and set the trace options before performing the actual trace.
|
Tool |
Description |
|---|---|
|
A Downstream Protective Device trace finds all protective devices downstream of the flag, by phase. The trace stops at an open switch. Select specific features to be traced in the ArcFM Electric Trace Options (Electric Traces tab). The trace operation executes as follows:
|
|
|
An Upstream Protective Device trace finds all protective devices upstream of the flag, by phase. The trace stops at the circuit source. Select specific features to be traced in the ArcFM Electric Trace Options (Electric Traces tab). The trace operation executes as follows:
|
|
|
The Electric Distribution trace finds all features connected to the same feeder system, by phase. If you change the status of a switch or breaker, an Electric Distribution trace will return all features affected by the status change. The trace operation executes as follows:
|
|
|
A Downstream Trace finds all features (lines and devices) in a feeder system by phase that are downstream of the trace flag. The trace operation executes as follows:
|
|
|
An Upstream Trace finds all features (lines and devices) in a feeder system by phase that are upstream of the trace flag. This trace requires Feeder Manager be configured. If you have configured Electric Tracing without Feeder Manager, this trace will not work. The trace operation executes as follows:
|
|
|
The Next Upstream Protective Device Trace finds the immediate protective device upstream of the flag. When you place a second flag, this trace marks the previously found protective device in gray. Use the ArcFM Electric Trace Options (Electric Traces tab) to specify which features are considered protective devices. The trace operation executes as follows:
|
|
|
The Isolation Protective Device trace finds protective devices immediately upstream and downstream of the flag. When you place a second flag, this trace marks the previously found protective devices in gray. Use the ArcFM Electric Trace Options (Electric Traces tab) to specify which features are considered protective devices. The trace operation executes as follows:
|
|
|
This button removes all flags and barriers from the map. It also clears the results if you have selected the Results as Drawings option. If you choose to view your results as a selected set, the Selection tab of the Attribute Editor will NOT be cleared. |
|
|
Use this toggle button to elect whether to zoom to the trace results. When this button is depressed (or toggled on), the map view will zoom to the trace results. |
|
|
Click this button to set various options for your electric trace. |