Circuit Trace

The circuit trace report shows splice points, fibers, and end devices that are part of the circuit.

IMPORTANT:
  • Make sure the web browser settings allow the display of blocked content. See your web browser help to determine how to set the display features.

  • Make sure the resolution is set correctly. Higher resolutions, such as 1680x1050, may cause the report to display in a less than optimum manner. See your web browser help to determine how to set the display features. 

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?