Ink

These settings control the size and color of the lines drawn with the Ink tool. Enter a value between 1 and 10 in the Pen Size field to determine the thickness of the line drawn with the Ink tool. Click the color square on the Pen Color field to select the color of the pen stroke.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?