Locator Tools
The Locator tool provides efficient and
varied methods for finding features on the map. The Locator finds
the specified object and related objects.
You can use the Add to Selection utility to add features in the results list to the Selection tab of the Attribute Viewer. Right-click the layer and choose Add to Selection to select the entire layer. Right-click tools also allow you to zoom to the selected feature and highlight it. If the Locator form is hiding a highlighted feature, the form becomes transparent to make the highlighted feature visible when it flashes.
The Locator Tool remembers the last locator selected as well as the status of the options (Auto Zoom and Auto Add to Selection).
Following is a list of the locators provided with the installation of ArcFM Viewer for ArcGIS Engine.
No matter which locator you choose, all have a Stop button. Each time you begin a search by clicking Find, the middle button on the user interface becomes Stop. Click Stop to cancel the search before it is finished. When the search is complete (or cancelled), the middle button reverts to Clear, which empties the results displayed in the bottom portion of the Locator tool's user interface as well as any search criteria.