Graphics Tab

The Graphics tab allows you to store graphic elements for placement on the map. Graphic favorites may be placed without an edit session started. To view the Graphics tab, select View > Graphics.

The Active Annotation Target tool provides the flexibility to place graphics in two different formats: graphic and annotation. 

 

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?