Electric Traces

Electric trace tasks allow you to check how current is flowing through a network of connected features. With ArcFM’s enhancements, you can define the upstream or downstream protective devices you want to find and indicate phase configurations for tracing electric distribution throughout the network. With these options, you can strategically tailor a variety of custom analysis tasks to specific implementations.

You may set the buffer threshold, modify the size of the buffer or turn it off altogether using the Tracing tab in the ArcFM Viewer Options. If the number of elements exceeds 10,000, the buffer is not drawn. As the number of elements approaches 10,000, the buffer may take longer to draw.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.