Welcome and FAQs

Welcome to the ArcFM Viewer for ArcGIS Engine Using Guide.

Here are some tips to help you find relevant information fast:

  • Topics are organized thematically in the Table of Contents along the left-hand side. Expand topics to reveal subtopics.

  • Use the Search field to type keywords you’re looking for. The Search defaults to querying within the current guide, but it also gives you the chance to query the entire catalog of guides. Further, it allows you to filter by product, guide type, and version. Enter your search terms to get started.

    Watch this short video that walks you through how to perform a search and filter your results.

  • While reading a topic, press the down key to scroll down through the topic, press the right key to move to the next topic in the Table of Contents, and press the left key to move to the previous topic in the Table of Contents.

  • Want to send a topic to a co-worker? Click the Sharable Link tool. This copies the current topic’s URL straight to your clipboard, ready for you to paste into an email or other message.

    Want to see how the Shareable Link tool works in action? Watch this short video!

  • Is the image a little too small? Click it to open in a separate tab. It opens as large as possible.

  • Use the “Was this helpful?” feedback options to drop us a note! Your comments help us improve documentation so you can get your job done most effectively. The following video explains how the “Was this helpful?” button works.

  • Watch this video to learn more about navigating the ArcFM Solution Documentation Portal.


Frequently Asked Questions (FAQ)

What’s the user community searching for? Here are the top searches and topics visited in this guide:

Engine Using and Config
  1. I can't find ArcFM Viewer when I open ArcMap. Where can I locate it?

    1. ArcFM Viewer runs independent of ArcMap, so it is not opened through ArcMap (like ArcFM). Instead, you can select ArcFM Viewer for ArcGIS Engine from the ArcFM Solution folder on the Start Menu.

  2. Why can't I edit custom classes feature classes in ArcFM Viewer for ArcGIS Engine?

    1. Relationship classes, feature-linked annotation, dimension feature classes, and custom feature classes require a Geodatabase Update Extension license from Esri in order to edit them. You will need to request that license from Esri.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.