Fiber Viewer Toolbar
The Fiber Viewer toolbar provides the tools to view fiber optic network data and produce reports. The following example depicts a toolbar containing all available icons and tools. Your toolbar may look different depending on your specific toolbar configuration.
| Tool | Description |
|---|---|
|
The Fiber Trace highlights an end-to-end path of connected fibers, and can generate a report about that path. |
|
|
Use the Optical Time Domain Reflectometer (OTDR) Trace to highlight a specified distance along a path of connected fibers. You can also use it to generate a report about that path. |
|
|
Clear the highlighted results of an OTDR trace or a Circuit Manager trace. |
|
|
Use the Possible Paths Tool to trace all available routes between two points in the fiber network using trace criteria that you define and to determine the availability of fibers in your network. |
|
|
The Patch Panel Connection Report generates an HTML report of attributes and connections for single or multiple pieces of equipment (such as a patch panel) in locations that you specify. |
|
|
The Splice Report generates a color-coded textual report of all the splices that exist at a single splice point. |
|
|
The Fiber Allocation Report provides a graphical display of the connections between every fiber in a fiber optic cable that is part of a selected set. |
|
|
Use the Glass Report to summarize characteristics of fiber optic cables that are part of a selected set of cables in the fiber optic network or on the entire network of fiber optic cables. |