Extensions Tab

This tab allows you to easily check out an ArcGIS Network Analyst Extension license. If you're using the Direction Search tool with a geodatabase, this license is necessary. If you're using the Direction Search tool with StreetMap data, this option must be unchecked.

This option is enabled only if you have a valid ArcGIS Network Analyst license. Ensure you have a valid license before attempting to use Network Analyst with the Direction Search tool.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?