Workflow Manager Toolbar

The following tools are available in Workflow Manager. A subset of these tools is available in the standalone version of Workflow Manager.

The following tasks reside only on the Available Tasks list:

  • Write Out CIM XML Message (Get)

  • Unlock Design

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?