Long-Start Motor Protection
Presentation
Long-start motor protection provides additional protection:
-
For machines at risk of difficult starting:
-
High inertia machines
-
High resistive torque machines
-
Machines with fluctuating load from steady state
Examples of machines with a significant risk of difficult starting: fans, compressors.
-
-
To avoid no-load starts:
-
Load not present
-
Machines oversized for the application
-
Description
Long-start motor protection is activated as soon as the average motor current Iavg exceeds 10% of the Ir setting value: the protection tlong time delay is actuated. Long-start motor protection compares the value of the average motor current Iavg with the setting value of the protection Ilong pickup.
By default, long-start motor protection is not active.
After function setting, long-start motor protection is:
-
Active during startup
-
Not active in steady state
Operating Principle (Difficult Starting)
On starting, the average motor current Iavg overruns the long-start motor protection Ilong pickup. The protection remains active as long as the average motor current Iavg has not fallen below the Ilong pickup.

1 Motor current
2 Activation of long-start motor protection tlong time delay
White: Protection not active. Green: Protection active
The curve can evolve in one of two ways:
-
Diagram Ι: The average motor current Iavg has not fallen below the Ilong pickup before the end of the tlong time delay (starting with too large a load). Long-start motor protection trips:
-
A: Activation of protection time delay (10% of Ir pickup is exceeded).
-
B: Protection tripped at the end of the time delay.
-
-
Diagram ΙΙ: The average motor current Iavg falls below the Ilong pickup before the end of the tlong time delay (correct starting). Long-start motor protection does not trip:
-
A: Activation of protection time delay (10% of Ir pickup is exceeded).
-
D: Deactivation of protection.
-
Operating Principle (No-Load Starting)
On starting, the average motor current Iavg does not exceed the long-start motor protection Ilong pickup. The protection remains active as long as the value of the average current Iavg has not fallen below 10% of the Ir setting value.

1 Motor current
2 Activation of long-start motor protection time delay
White: Protection not active; Green: Protection active
Diagram ΙΙΙ: The motor current has not fallen below 10% of the Ir setting value before the end of the tlong time delay: long-start motor protection trips.
-
A: Activation of protection time delay (10% of Ir pickup is exceeded)
-
B: Protection tripped at the end of the time delay
If the motor current falls back below 10% of the Ir setting value before the end of the protection tlong time delay (for example on contactor opening), long-start motor protection does not trip.
Setting the Protection
The Ilong pickup and the tlong time delay settings can only be accessed:
-
With EcoStruxure Power Commission software (password-protected)
-
By sending a setting command using the communication network (password-protected)
Ilong Pickup Setting Value
The Ilong pickup setting value is in multiples of Ir.
The pickup setting range is 1–8 x Ir. The increment is 0.1 x Ir. The factory setting is OFF: protection not active.
The accuracy range is +/-10%.
tlong Time Delay Setting Value
The tlong time delay setting value is in seconds.
The tlong time delay setting range is 1–200 s. The increment is 1 s. The factory setting value for the time delay is 10 s.