DOCA0141EN-03

ComPact NSX100-250 - Distribution Protection

MicroLogic 5.2 and 6.2 A or E and 7.2 E Trip Units

MicroLogic 5.2 and 6.2 A or E, and 7.2 E

40–160 A

Reflex tripping

MicroLogic 5.2 and 6.2 A or E, and 7.2 E

250 A

Reflex tripping

MicroLogic 6.2 A or E (ground-fault protection)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?