Long-Time Protection
Presentation
Long-time protection on MicroLogic 5, 6, and 7 trip units protects electrical distribution applications against overload currents. It is identical for MicroLogic 5, 6, and 7 trip units.
Operating Principle
Long-time protection is I2t IDMT (Inverse Definite Minimum Time):
-
It incorporates the thermal image function.
-
It is set with the Ir pickup and as the tr trip time delay.
Setting the Long-Time Protection
Set the Ir pickup as follows:
-
With the MicroLogic trip unit Ir dial to preset the value and the keypad to fine-tune the value
-
With EcoStruxure Power Commission software (password-protected)
-
By sending a setting command using the communication network (password-protected)
Set the time delay tr as follows:
-
With the keypad on the MicroLogic trip unit
-
With EcoStruxure Power Commission software (password-protected)
-
By sending a setting command using the communication network (password-protected)
Ir Pickup Setting Values
The long-time protection tripping range is 1.05–1.20 Ir according to standard IEC/EN 60947-2.
The default Ir pickup setting value is the maximum dial position In.
The following table shows the Ir pickup value preset on the dial:
|
In rating |
Preset values of Ir (A) depending on the trip unit In rating and the dial position |
||||||||
|---|---|---|---|---|---|---|---|---|---|
|
40 A |
18 |
18 |
20 |
23 |
25 |
28 |
32 |
36 |
40 |
|
100 A |
40 |
45 |
50 |
55 |
63 |
70 |
80 |
90 |
100 |
|
160 A |
63 |
70 |
80 |
90 |
100 |
110 |
125 |
150 |
160 |
|
250 A |
100 |
110 |
125 |
140 |
150 |
175 |
200 |
225 |
250 |
|
400 A |
160 |
180 |
200 |
230 |
250 |
280 |
320 |
360 |
400 |
|
630 A |
250 |
280 |
320 |
350 |
400 |
450 |
500 |
570 |
630 |
The accuracy range is + 5%/+ 20%.
Use the keypad to fine-tune the setting, in increments of 1 A:
-
The setting range maximum is the preset value of the dial.
-
The range minimum is 0.9 times the minimum preset value (for the 400 A rating, the setting range minimum is 100 A).
Example: A MicroLogic 5.2 trip unit rated In = 250 A is preset by the dial at 140 A:
-
The minimum preset value is 100 A
-
The keypad fine-tuning range is 90–140 A
tr Time Delay Setting Values
The setting value displayed is the value of the trip time delay for a current of 6 x Ir.
The default tr time delay setting value is 16 (maximum value) that is, 16 s at 6 x Ir.
The following table shows the value of the trip time delay (in seconds) according to the current in the load for the setting values displayed on-screen:
|
Current in the load |
tr Trip time delay per setting value |
|||||
|---|---|---|---|---|---|---|
|
0.5 |
1 |
2 |
4 |
8 |
16 |
|
|
1.5 x Ir |
15 s |
25 s |
50 s |
100 s |
200 s |
400 s |
|
6 x Ir |
0.5 s |
1 s |
2 s |
4 s |
8 s |
16 s |
|
7.2 x Ir |
0.35 s |
0.7 s |
1.4 s |
2.8 s |
5.5 s |
11 s |
The accuracy range is -20%/+0%.
Thermal Image
The trip unit uses the calculation of a thermal image to evaluate the conductor heat rise and precisely monitor the thermal state of the conductors.
Example:
Comparison of the heat rise calculation without thermal image (diagram A) and with thermal image (diagram B):

0 Instantaneous current (cyclical) in the load
1 Conductor temperature
2 Current calculated without thermal image (diagram A), with thermal image (diagram B)
3 Long-time protection pickup: Ir
-
Trip unit without thermal image: On each current pulse, the trip unit only considers the thermal effect on the pulse under consideration. No tripping occurs despite the build-up in conductor heat rise.
-
Trip unit with thermal image: The trip unit adds the thermal effect of successive current pulses. Tripping occurs based on the actual thermal state of the conductor.
Conductor Heat Rise and Tripping Curves
Use the analysis of the equation of heat rise in a conductor, through which a current I runs, to determine the nature of physical phenomena:
-
For low- or medium-intensity currents (I < Ir), the conductor equilibrium temperature (for an infinite time) only depends on the current quadratic demand value. The limit temperature corresponds to a limit current (Ir pickup for trip unit long-time protection).
-
For low overcurrents (Ir < I < Isd), the conductor temperature only depends on the I2t energy provided by the current. The limit temperature is an I2t IDMT curve.
-
For high overcurrents (I > Isd), the phenomenon is identical if the I2t function of the short-time protection is active (I2t ON).
Thermal Memory
MicroLogic 5, 6, and 7 trip units incorporate the thermal memory function which ensures that the conductors are cooled even after tripping. Cooling lasts for 20 minutes before or after tripping.