DOCA0141EN-03

Alarms on a Trip, Failure, and Maintenance Event

Presentation

Alarms on a trip, failure, and maintenance event are always active. They can be accessed:

  • Using the communication network

  • On the FDM121 display

Certain alarms can be assigned to an SDx module output by using EcoStruxure Power Commission software.

Alarm Setup

The functions of alarms on a trip and failure event are fixed and cannot be modified.

The functions of the two maintenance alarms (OF operation overrun counter threshold and Close command counter threshold) can be modified:

  • With EcoStruxure Power Commission software (password-protected)

  • By sending a setting command using the communication network (password-protected)

Alarm Priority Level

Assign each alarm a priority level:

  • High priority

  • Medium priority

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?