DOCA0141EN-03

Circuit Breaker Communication

Presentation

ComPact NSX circuit breakers with MicroLogic 5, 6, and 7 trip units can be integrated into a communication network using Modbus protocol. Use data transmitted by the communication network to provide supervision and monitoring for an installation.

Modbus communication offers the options of:

  • Reading remotely:

    • The circuit breaker status

    • Measurements

    • Operating assistance information

  • Controlling the circuit breaker remotely.

For more information about the Modbus communication network, refer to DOCA0091EN ComPact NSX - Modbus Communication Guide.

Remote Readout of the Circuit Breaker States

Remote readout of the circuit breaker status is accessible by all ComPact NSX circuit breakers equipped with a BSCM. The following data is available using the communication network:

  • Open/closed position (OF)

  • Trip indicator (SD)

  • Electrical fault indicator (SDE)

For more information, refer to DOCA0140EN ComPact NSX - Circuit Breakers and Switch-Disconnectors 100–630 A - User Guide.

Remote Readout of the Measurements

Access the measurement readout with MicroLogic 5, 6, and 7 trip units.

For more information about measurements, refer to the metering function.

Remote Readout of the Operating Assistance Information

Access the operating assistance readout with MicroLogic 5, 6, and 7 trip units. The following operating assistance information is available:

Circuit Breaker Remote Control

The circuit breaker remote control is accessible by any circuit breaker with a MicroLogic trip unit, a BSCM, and a communicating motor mechanism. The following commands are available using the communication network:

  • Circuit breaker opening

  • Circuit breaker closing

  • Circuit breaker reset

For more information, refer to DOCA0140EN ComPact NSX - Circuit Breakers and Switch-Disconnectors 100–630 A - User Guide.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.