Protection for Motor-Feeders
Presentation
MicroLogic 6 E-M trip units on ComPact NSX circuit breakers:
-
Provide protection for direct-on-line motor-feeders (direct-on-line starting is the most widely used type of motor-feeder).
-
Integrate the basic protections (overload, short-circuit, and phase unbalance) for the motor-feeder and additional protections and/or specific options for motor applications.
-
Allow protection and coordination of the motor-feeder components that comply with the requirements of standard IEC/EN 60947-2 and IEC/EN 60947-4-1. For more information, refer to DOCA0140EN ComPact NSX - Circuit Breakers and Switch-Disconnectors 100–630 A - User Guide.
Description
ComPact NSX circuit breakers equipped with the MicroLogic 6 E-M trip unit can be used to create motor-feeders with two devices.

A ComPact NSX circuit breaker equipped with a MicroLogic 6 E-M trip unit
B Short-circuit protection
C Overload protection
D Ground-fault current protection
E Contactor
F SDTAM Module Option
Operating States
The MicroLogic 6 E-M trip unit considers the application to be operating as soon as the 10% of Ir pickup is crossed in a positive direction by the motor current.
Two operating states are considered:
-
Startup state
-
Steady state
Startup State
The MicroLogic 6 E-M trip unit considers the application to be in startup state according to the following criteria:
-
Start: As soon as the 10% of Ir pickup is crossed in a positive direction by the motor current
-
End: As soon as the Id pickup is crossed in a negative direction or at maximum after a td time delay defined as follows:
-
If long-start protection is not activated (factory setting), the Id pickup equals 1.5 x Ir and the td time delay equals 10 s (non-adjustable parameters).
Exceeding the 10 s time delay does not result in tripping.
-
If long-start protection is activated, the Id pickup equals Ilong and the td time delay equals tlong (adjustable parameters).
Exceeding the tlong time delay results in long-start protection tripping.
-
Steady State
The MicroLogic 6 E-M trip unit considers the application to be in steady state according to the following criteria:
-
Start: As soon as startup ends
-
End: As soon as the 10% of Ir pickup is crossed in a negative direction by the motor current
Operating Diagram
The following diagram shows the two operating states for a motor application:

A ComPact NSX circuit breaker status (green = ON position)
B Contactor status (green = ON position)
C Current in the motor application
Operating states:
D: Startup state
E: Steady state (the active states are shown in green)
Protection Functions
|
Item |
Parameter |
Description |
Adjustable |
|
|---|---|---|---|---|
|
0 |
In |
Trip unit setting range: Minimum setting/maximum setting = trip unit In rating |
No |
|
|
1 |
Ir |
Long-time protection pickup |
L |
Yes |
|
2 |
Cl |
Long-time protection trip class |
Yes |
|
|
3 |
Isd |
Short-time protection pickup |
S |
Yes |
|
4 |
tsd |
Short-time protection time delay |
No |
|
|
5 |
Ii |
Instantaneous protection pickup |
I |
No |
|
6 |
Ig |
Ground-fault protection pickup |
G |
Yes |
|
7 |
tg |
Ground-fault protection time delay |
Yes |
|
|
|
Iunbal |
Phase unbalance protection pickup |
Yes |
|
|
|
tunbal |
Phase unbalance protection time delay |
Yes |
|
Each function is reviewed in detail on the following pages.
Additional Protection
The MicroLogic 6 E-M trip unit incorporates additional protection functions for motor applications.
|
Protection |
Default Activation |
Default Setting |
SDTAM Activation |
|---|---|---|---|
|
Motor jam protection |
OFF |
Ijam: OFF, tjam: 5 s |
Yes |
|
Underload motor protection |
OFF |
Iund: OFF, t und: 10 s |
Yes |
|
Long-start motor protection |
OFF |
Ilong: OFF, tlong: 10 s |
No |
The additional protections are activated for startup or steady state or in both cases.
Setting the Protection
Set the protection functions:
-
On the MicroLogic trip unit, by using the adjustment dials and the keypad (depending on the protection function and the MicroLogic type).
-
With EcoStruxure Power Commission software (password-protected)
-
By sending a setting command using the communication network (password-protected)
Reflex Tripping
In addition to the protection functions integrated in the MicroLogic trip units, ComPact NSX circuit breakers have reflex protection. This system breaks very high fault currents by mechanically tripping the device with a “piston” actuated directly by the pressure produced in the circuit breaker from a short-circuit. This piston operates the opening mechanism, resulting in ultra-fast circuit breaker tripping.
SDTAM Module Option
The SDTAM module early tripping function can be used to command contactor opening 400 ms before the calculated circuit breaker tripping in the case of:
-
Long-time protection
-
Phase unbalance protection
-
Motor jam protection
-
Underload motor protection
The contactor can be closed again automatically or manually depending on the setting of the SDTAM module. For more information, refer to DOCA0140EN ComPact NSX - Circuit Breakers and Switch-Disconnectors 100–630 A - User Guide.
Example of Using the SDTAM Module
The following figures illustrate operation of the Motor jam protection without the SDTAM module (diagram Ι) and with the SDTAM module (diagram ΙΙ):

1 ComPact NSX circuit breaker status
White: Open; Green: Closed; Black: Tripped
2 Contactor status (SD contact in the contactor coil)
White: Open; Green: Closed
3 Motor current
4 Monitoring by motor jam protection
White: Not active (startup state). Green: Active (steady state)
Analysis of Operation
The following table describes operation without the SDTAM module (diagram Ι).
|
Event |
Comments |
|---|---|
|
A |
Application motor switches to steady state. Motor jam protection monitoring is activated. |
|
B |
Occurrence of an overload current on the application (for example, rotor braked due to high viscosity of one of the mixing fluids) The Motor jam protection tjam time delay is actuated as soon as the motor current crosses the Ijam pickup. |
|
C |
End of Motor jam protection time delay Motor jam protection causes the ComPact NSX circuit breaker to trip. |
|
D |
Application returned to service manually after the motor has cooled and the circuit breaker has closed again. |
The following table describes operation with the SDTAM module (diagram ΙΙ).
|
Event |
Comments |
|---|---|
|
A |
Identical to diagram Ι |
|
B |
Identical to diagram Ι |
|
C |
400 ms before the end of the Motor jam protection time delay, the SDTAM module:
Both outputs are activated for a time delay (which can be set between 1 and 15 minutes). |
|
D |
Application contactor returned to service automatically: the time delay allows the motor to cool down. |
The SDTAM module can be set to the OFF position: the application is returned to service manually (by deactivating the SDTAM module power supply).