Indication on the MicroLogic Display
Presentation
Indication screens indicate the status of the installation.
Maintenance interventions should be executed according to the priority level:
-
Configured (alarms: high, medium, low, or no priority)
-
Pre-defined (trip and failure events: high or medium priority)
Stacking Screens
When a number of events arrive simultaneously, they stack according to their criticality level: 0 (no criticality) to 4 (high criticality).
|
Criticality |
Screen (1) |
|---|---|
|
0 |
Main screen |
|
1 |
Outx alarm screen |
|
2 |
Err internal failure screen |
|
3 |
Stop internal fault screen |
|
4 |
Trip screen |
|
(1) The screens and their acknowledgment procedure are described below. |
|
Example:
An alarm on a voltage measurement Outx, then an internal failure occurred:
-
The screen displayed is the internal failure screen (Criticality = 2).
-
After acknowledging the internal failure screen, the alarm Outx screen is displayed (Criticality = 1).
-
After acknowledging the internal failure Outx screen, the main screen is displayed (Criticality = 0).
The same acknowledgment sequence should be performed if the internal failure occurred before the voltage measurement Outx.
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
CAUTION |
|---|
|
HAZARD OF INCORRECT INFORMATION
If the trip unit displays an Err screen, replace the MicroLogic trip unit at the next regular maintenance.
Failure to follow these instructions can result in injury or equipment damage.
|
Indication of Correct Installation Operation
Alarm Indication
Circuit breaker with SDx module option
|
Screen |
Cause |
|---|---|
|
An alarm configured on the SDx module in permanent latching mode has not been acknowledged or the acknowledgment request is made when the alarm is still active. |
Check the cause of the alarm and acknowledge the alarm
by pressing the
key twice (validation and
confirmation).
The main screen (current value of the most heavily loaded phase) is displayed.
Indication of Faults With MicroLogic 5, 6, and 7 Trip Units
For more information about definitions of the protections associated with indications, refer to the electrical distribution protection.
|
Screen |
Cause |
|---|---|
|
Tripped by long-time protection: Up arrow pointing to Ir, breaking value displayed |
|
|
Tripped by short-time protection: Up arrow pointing to Isd, breaking value displayed |
|
|
Tripped by instantaneous protection or reflex protection: Up arrow pointing to Ii, breaking value displayed |
|
|
Tripped by integrated instantaneous protection: Up arrow pointing to Ii, triP displayed |
|
|
MicroLogic 6 trip unit Tripped by ground-fault protection: Up arrow pointing to Ig, triP displayed |
|
|
MicroLogic 7 with integrated earth-leakage protection Tripped by earth-leakage protection: Up arrow pointing to IΔn |
|
|
Tripped due to lack of ENCT option, as the ENCT option was declared during the protection function settings of the MicroLogic trip unit. Install the ENCT option or connect a jumper between terminals T1 and T2 on the MicroLogic trip unit. |
Indication of Faults With MicroLogic 6 E-M Trip Unit
For more information about definitions of the protections associated with indications, refer to the protection for motor-feeders.
|
Screen |
Cause |
|---|---|
|
Tripped by long-time protection: Up arrow pointing to Ir, triP displayed (1) |
|
|
Tripped by short-time protection: Up arrow pointing to Isd, breaking value displayed |
|
|
Tripped by instantaneous protection or reflex protection: Inst displayed |
|
|
Tripped by ground-fault protection: Up arrow pointing to Ig, triP displayed |
|
|
Tripped by unbalance protection: Up arrow pointing to Iunbal, triP displayed (1) |
|
|
Tripped by jam motor protection: Up arrow pointing to Ijam, triP displayed (1) |
|
|
Tripped by underload protection: Undl displayed (1) |
|
|
Tripped by long-start protection: Strt displayed |
|
|
(1) These trip causes can be managed automatically by SDTAM output 2 (OUT2) action on the contactor. |
|
Acknowledging the Trip Screens
Acknowledge the trip screens by pressing the
key twice (validation and
confirmation).
WARNING |
|---|
|
HAZARD OF CLOSING ON ELECTRICAL FAULT
Do not close the circuit breaker again without first inspecting
and, if necessary, repairing the downstream electrical equipment.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
The fact that a protection has tripped does not remedy the cause of the fault on the downstream electrical equipment.
|
Step |
Action |
|---|---|
|
1 |
Isolate the feed before inspecting the downstream electrical equipment. |
|
2 |
Look for the cause of the fault. |
|
3 |
Inspect and, if necessary, repair the downstream equipment. |
|
4 |
Inspect the equipment in the event of a short-circuit trip. |
|
5 |
Reset and close the circuit breaker again. |
For more information about troubleshooting and restarting following a fault, refer to DOCA0140EN ComPact NSX - Circuit Breakers and Switch-Disconnectors 100–630 A - User Guide.
Indication of a Minor Internal Malfunction of the MicroLogic Trip Unit
|
Screen |
Cause |
|---|---|
|
A minor internal malfunction on the MicroLogic trip unit, whether temporary or permanent, has occurred without the circuit breaker tripping (the failure does not affect the trip unit protection functions). |
CAUTION |
|---|
|
HAZARD OF INCORRECT INFORMATION
Replace the MicroLogic trip unit at the next maintenance interval.
Failure to follow these instructions can result in injury or equipment damage.
|
Acknowledging the Screen
Acknowledge
the screen by
pressing the key twice
(validation and confirmation):
-
The Mode key can access the measurements and settings.
-
The screen becomes the main screen if the failure is permanent.
Indication of a Major Internal Malfunction of the MicroLogic Trip Unit
|
Screen |
Cause |
|---|---|
|
A major internal malfunction has occurred in the MicroLogic trip unit. This fault trips the circuit breaker. |
CAUTION |
|---|
|
HAZARD OF INCORRECT INFORMATION
Replace the MicroLogic trip unit immediately.
Failure to follow these instructions can result in injury or equipment damage.
|
Acknowledging the Screen
The screen cannot be acknowledged
with the
key:
-
It is no longer possible to close the circuit breaker
-
The Mode key cannot access the measurements and settings
-
The screen becomes the main screen
Screen Firmware Download Indication
|
Screen |
Cause |
|---|---|
|
The MicroLogic trip unit is waiting for, or is downloading, the firmware through EcoStruxure Power Commission software (duration: 3 minutes approximately).
If the message persists after several download attempts, replace the MicroLogic trip unit. |
DANGER
CAUTION
















WARNING