Ground-Fault Protection
Presentation
Ground-fault protection on MicroLogic 6 trip units protects all types of electrical distribution applications against ground-fault currents in the TN-S system.
For more information on ground-fault currents, refer to DOCA0140EN ComPact NSX - Circuit Breakers and Switch-Disconnectors 100–630 A - User Guide.
Operating Principle
Ground-fault protection is definite time:
-
It includes the possibility of an I2t inverse time curve function.
-
Set as Ig pickup and as tg trip time delay.
Setting the Ground-Fault Protection
Set the Ig pickup:
-
With the MicroLogic 6 trip unit Ig dial to preset the value and with the keypad to fine-tune the value
-
With EcoStruxure Power Commission software (password-protected)
-
By sending a setting command using the communication network (password-protected)
Set the tg time delay:
-
With the keypad on the MicroLogic 6 trip unit
-
With EcoStruxure Power Commission software (password-protected)
-
By sending a setting command using the communication network (password-protected)
The tg time delay setting includes activation/deactivation of the I2t function.
Ig Pickup Setting Values
The Ig pickup setting value is in multiples of In.
The default Ig pickup setting value is the same as the minimum value read on the dial:
-
0.40 x In for trip units rated 40 A
-
0.20 x In for trip units rated > 40 A
Ground-fault protection can be deactivated by setting the Ig dial to the OFF position.
Ground-fault protection can be reactivated even with the Ig dial in the OFF position:
-
By fine-tuning on the keypad
-
With EcoStruxure Power Commission software (password-protected)
-
By sending a setting command using the communication network (password-protected)
The following two tables specify the setting values (preset by a dial) and setting ranges (set on the keypad.)
On the keypad, the increment is 0.05 x In.
For trip units rated 40 A
|
Type of setting |
Value or setting range (x In) |
||||||||
|---|---|---|---|---|---|---|---|---|---|
|
Preset by a dial |
0.40 |
0.40 |
0.50 |
0.60 |
0.70 |
0.80 |
0.90 |
1 |
OFF |
|
Setting range on the keypad |
0.40 |
0.40 |
0.4–0.5 |
0.4–0.6 |
0.4–0.7 |
0.4–0.8 |
0.4–0.9 |
0.4–1 |
0.4–1 + OFF |
For trip units rated > 40 A
|
Type of setting |
Value or setting range (x In) |
||||||||
|---|---|---|---|---|---|---|---|---|---|
|
Preset by a dial |
0.20 |
0.30 |
0.40 |
0.50 |
0.60 |
0.70 |
0.80 |
1 |
OFF |
|
Setting range on the keypad |
0.20 |
0.2–0.3 |
0.2–0.4 |
0.2–0.5 |
0.2–0.6 |
0.2–0.7 |
0.2–0.8 |
0.2–1 |
0.2–1 + OFF |
The accuracy range is +/-10%.
tg Time Delay Setting Values
The tg time delay setting value is in seconds. The hold and breaking times are in milliseconds.
The default tg time delay setting value is 0 s with I2t OFF.
The following table shows the setting values of tg time delay in seconds (s) with the I2t function active (I2t ON) or not active (I2t OFF). The associated hold and breaking times are shown in milliseconds (ms):
|
Function |
Setting value |
||||
|---|---|---|---|---|---|
|
tg with I2t OFF (s) |
0 |
0.1 |
0.2 |
0.3 |
0.4 |
|
tg with I2t ON (s) |
– |
0.1 |
0.2 |
0.3 |
0.4 |
|
Hold time (ms) |
20 |
80 |
140 |
230 |
360 |
|
Maximum breaking time (ms) |
80 |
140 |
200 |
320 |
500 |
I2t Inverse Time Curve Function
The I2t inverse time curve function for ground-fault protection operates in the same way as the I2t inverse time curve function for short-time protection.
Testing the Ground-Fault Protection
The ground-fault protection can be tested to check the electronic tripping function of the trip unit. Use the keypad of the MicroLogic 6 trip unit to perform this test.
The ground-fault protection test can be performed with the padlock
locked
or unlocked
.
Follow these steps to test and reset the ground-fault protection on MicroLogic 6 trip units.
|
Step |
Action |
Display |
|---|---|---|
|
1 |
Provide a power supply to the trip unit so that the screen displays the result of the test after the circuit breaker trips. |
– |
|
2 |
Select the Instantaneous measurement readout mode (the display is the most heavily loaded phase, in this example Phase 2). |
|
|
3 |
Select the ground-fault current measurement screen (the value is a percentage of the Ig setting). |
|
|
4 |
Access the ground-fault protection test function by pressing . The pictogram appears and the pictogram blinks. |
|
|
5 |
Prompt the ground-fault protection test by pressing . The circuit breaker trips. The ground-fault protection trip screen is displayed. |
|
|
6 |
Acknowledge the ground-fault trip screen by pressing . The pictogram blinks. |
|
|
7 |
Confirm by pressing again. The confirmation displays for 2 s. |