DOCA0141EN-03

Instantaneous Protection

Presentation

Instantaneous protection on MicroLogic 5, 6, and 7 trip units protects all types of electrical distribution applications against very high short-circuit currents.

It is identical for MicroLogic 5, 6, and 7 trip units.

Operating Principle

Instantaneous protection is definite time, set as Ii pickup and without a time delay.

The instantaneous protection setting is:

  • Ii: instantaneous protection pickup

Setting the Instantaneous Protection

Set the Ii pickup:

  • With the keypad on the MicroLogic trip unit

  • With EcoStruxure Power Commission software (password-protected)

  • By sending a setting command using the communication network (password-protected)

Ii Pickup Setting Values

The Ii pickup setting value is in multiples of In.

The default Ii pickup setting value is the maximum setting value (15, 12, or 11 x In according to trip unit In rating)

The following table shows the setting ranges and increments according to the MicroLogic trip unit In rating.

Trip unit In rating

Setting range

Increments

100 A and 160 A

1.5–15 x In

0.5 x In

250 A and 400 A

1.5–12 x In

0.5 x In

630 A

1.5–11 x In

0.5 x In

The accuracy range is +/-10%.

The hold time is 10 ms.

The maximum breaking time is 50 ms.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?