Schematics with ComPacT NSX Circuit Breakers
General Description
Depending on the BSCM Modbus SL/ULP module mode used, the user must connect the BSCM Modbus SL/ULP module using one of the following configurations:
-
Connection of the BSCM Modbus SL/ULP module to the Modbus SL hub
-
Connection of the BSCM Modbus SL/ULP module to an IFM or IFE communication interface
For more information, refer to ULP System User Guide.
BSCM Modbus SL Only Mode
In Modbus SL only mode, the BSCM Modbus SL/ULP module is used to connect the ComPacT NSX circuit breaker to the Modbus Serial Line communication network by using a Modbus SL hub with commercial reference LV434224. To read the SD status on the BSCM Modbus SL/ULP module, use the SD auxiliary contact for BSCM Modbus SL/ULP module with commercial reference LV434210.
The figure below illustrates an example of the BSCM Modbus SL/ULP module in Modbus SL only mode.
BSCM Modbus SL and ULP Mode
In Modbus SL and ULP mode, the BSCM Modbus SL/ULP module is used to connect the ComPacT NSX circuit breaker to:
-
The Modbus Serial Line communication network via a Modbus SL hub
-
ULP modules such as IO module 1, IO module 2, FDM121 display via NSX cord
The figure below illustrates an example of the BSCM Modbus SL/ULP module in Modbus SL and ULP mode.
-
Modbus TCP client
-
Ethernet cable
-
Modbus SL hub (LV434224)
-
Modbus SL cord (LV434221, LV434222, or LV434223)
-
BSCM Modbus SL/ULP module (LV434220)
-
MicroLogic 5, 6, or 7 trip unit
-
NSX cord (LV434200, LV434201, LV434202, or LV434204)
-
IFE Ethernet switchboard server (LV434002)
-
ULP cord (LV434195, LV434196, LV434197, or LV434198)
-
IO module (LV434063)
-
FDM121 display (TRV00121)
BSCM ULP Only Mode
In ULP only mode, the BSCM Modbus SL/ULP module is used to connect the ComPacT NSX circuit breaker to ULP modules such as IFM or IFE communication interface, via ULP communication network using NSX cord. Other ULP modules such as the IO module and the FDM121 display can also be connected to the same ULP communication network.
DANGER |
|---|
|
hazard of electric shock, explosion or arc flash
Failure to follow these instructions will result in death or serious injury.
|
The ULP only mode is recommended to connect plug-in or withdrawable ComPacT NSX circuit breakers to a communication network, by using an IFM or IFE communication interface.
The BSCM Modbus SL/ULP module with commercial reference LV434220 in ULP only mode replaces the BSCM module with commercial reference LV434205.
The figure below illustrates an example of the BSCM Modbus SL/ULP module in ULP only mode.
-
Modbus TCP client
-
Ethernet cable
-
IFE Ethernet interface for one circuit breaker (LV434001) or IFE Ethernet switchboard server (LV434002)
-
BSCM Modbus SL/ULP module (LV434220)
-
MicroLogic 5, 6, or 7 trip unit
-
NSX cord (LV434200, LV434201, LV434202, or LV434204)
-
ULP cord (LV434195, LV434196, LV434197, or LV434198)
-
IO module (LV434063)
-
FDM121 display (TRV00121)
DANGER