DOCA0213EN-03

Trip History

General Description

The trip history registers describe the last 17 trips. The trip history format corresponds to a series of 17 records. Each record is composed of 7 registers describing one trip.

The trip history registers return 32768 (0x8000) when they are not used.

Trip Record Number

A read request of 7x(n) registers is necessary to read the last n trip records, where 7 is the number of registers for each trip record.

For example, a read request of 7 x 4 = 28 registers is necessary to read the last 4 trip records of the trip history:

  • The first 7 registers describe the first trip record (most recent trip).

  • The next 7 registers describe the second trip record.

  • The last 7 registers describe the third trip record.

  • The last 7 registers describe the fourth trip record.

Address

Register

Description

0x238B–0x2391

9100–9106

Trip record 1 (most recent trip)

0x2392–0x2398

9107–9113

Trip record 2

0x2399–0x239F

9114–9120

Trip record 3

0x23A0–0x23A6

9121–9127

Trip record 4

0x23A7–0x23AD

9128–9134

Trip record 5

0x23AE–0x23B4

9135–9141

Trip record 6

0x23B5–0x23BB

9142–9148

Trip record 7

0x23BC–0x23C2

9149–9155

Trip record 8

0x23C3–0x23C9

9156–9162

Trip record 9

0x23CA–0x23D0

9163–9169

Trip record 10

0x23D1–0x23D7

9170–9176

Trip record 11

0x23D8–0x23DE

9177–9183

Trip record 12

0x23DF–0x23E5

9184–9190

Trip record 13

0x23E6–0x23EC

9191–9197

Trip record 14

0x23ED–0x23F3

9198–9204

Trip record 15

0x23F4–0x23FA

9205–9211

Trip record 16

0x23FB–0x2401

9212–9218

Trip record 17 (oldest trip)

Trip Record

A read request of 7 registers is necessary to read a trip record.

The order and the description of the trip record registers are the same as that of the trip record 1:

Trip Record 1 (Most Recent Trip)

Address

Register

RW

X

Unit

Type

Range

Description

0x238B

9100

R

1

INT16U

0–65535

Trip code (see next paragraph)

0x238C–

0x238E

9101–

9103

R

ULP DATE

Date and time of event (trip or acknowledge Data Type: ULP DATE

0x238F

9104

R

1

INT16U

1–2

Event type

MSB = 0 (reserved)

Event occurrence: LSB = 1

Event completion: LSB = 2

0x2390

9105

R

1

INT16U

0–5

Faulty phase

0 = failure (no faulty phase)

1 = phase 1

2 = phase 2

3 = phase 3

4 = phase N

5 = phase 1 2 3 (motor application, ground-fault, earth-leakage)

0x2391

9106

R

1

A

INT16U

0–65535

Interrupted current (peak) (1)

(1) Measurement depends on the application:

  • For electrical distribution application, the interrupted current is measured when a trip occurs, due to the long-time protection, the short-time protection, or the instantaneous protection.

  • For motor-feeder application, the interrupted current is measured when a trip occurs, due to the short-time protection.

  • In case of other trip types, the interrupted current is not measured and the value recorded is 65535 (0xFFFF).

Trip Codes

Trip Code

Description

1000 (0x03E8)

Long-time protection Ir

1001 (0x03E9)

Short-time protection Isd

1002 (0x03EA)

Instantaneous protection Ii

1003 (0x03EB)

Ground-fault protection Ig

1004 (0x03EC)

Earth-leakage protection IΔn

1005–1009 (0x03ED–0x03F1)

Reserved

1010 (0x03F2)

Integrated instantaneous protection

1011 (0x03F3)

STOP (trip unit internal failure)

1012 (0x03F4)

Instantaneous with earth-leakage protection

1013–1031 (0x03F5–0x0407)

Reserved

1032 (0x0408)

Unbalance motor protection

1033 (0x0409)

Jam motor protection

1034 (0x040A)

Underload motor protection

1035 (0x040B)

Long-start motor protection

1036 (0x040C)

Reflex tripping protection

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?