User-Defined Alarms
General Description
EcoStruxure Power Commission software enables the configuration of 10 user-defined alarms that can be chosen from a list of 150 predefined alarms.
Each user-defined alarm has a corresponding user-defined alarm number (201–210) and a corresponding alarm code (see next paragraph).
Each alarm has a priority level that manages the alarm display on the FDM121 display:
-
No priority = N/A (not affected)
-
Low priority = 1. No alarm display on the FDM121 display.
-
Medium priority = 2. The FDM121 display LED is steady ON.
-
High priority = 3. The FDM121 display LED blinks and a pop-up screen informs the user the alarm is active.
For more information regarding the relationship between alarm priority and FDM121 display, refer to DOCA0188•• ComPacT NSX MicroLogic 5/6/7 Trip Units – User Guide.
The settings of the 10 user-defined alarms are in the user-defined alarms registers:
|
Address |
Register |
Description |
|---|---|---|
|
0x1A71–0x1A7C |
6770–6781 |
User-defined alarm 201 |
|
0x1A7D–0x1A88 |
6782–6793 |
User-defined alarm 202 |
|
0x1A89–0x1A94 |
6794–6805 |
User-defined alarm 203 |
|
0x1A95–0x1AA0 |
6806–6817 |
User-defined alarm 204 |
|
0x1AA1–0x1AAC |
6818–6829 |
User-defined alarm 205 |
|
0x1AAD–0x1AB8 |
6830–6841 |
User-defined alarm 206 |
|
0x1AB9–0x1AC4 |
6842–6853 |
User-defined alarm 207 |
|
0x1AC5–0x1AD0 |
6854–6865 |
User-defined alarm 208 |
|
0x1AD1–0x1ADC |
6866–6877 |
User-defined alarm 209 |
|
0x1ADD–0x1AE8 |
6878–6889 |
User-defined alarm 210 |
User-Defined Alarm Record
A read request of 12 registers is necessary to read a user-defined alarm record.
The order and the description of the user-defined alarms records are the same as that of user-defined alarm record 1:
|
User-Defined Alarm 201 |
|||||||
|---|---|---|---|---|---|---|---|
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|
0x1A71 |
6770 |
R |
– |
– |
INT16U |
– |
The MSB gives the activity of the alarm: 0 = On, 1 = Off. The factory setting is 1 (Off). The LSB gives the priority of the alarm: N/A, 1, 2, or 3. The factory setting is N/A (no priority). |
|
0x1A72 |
6771 |
R |
– |
– |
INT16U |
– |
Measurement identifier (1) |
|
0x1A73 |
6772 |
– |
– |
– |
– |
– |
Reserved |
|
0x1A74 |
6773 |
R |
1 |
(2) |
INT16 |
-32767– +32767 |
Threshold pick-up value. The factory setting is 0. |
|
0x1A75 |
6774 |
– |
– |
– |
– |
– |
Reserved |
|
0x1A76 |
6775 |
R |
1 |
s |
INT16U |
0–3000 |
Pick-up time delay. The factory setting is 0. |
|
0x1A77 |
6776 |
R |
1 |
(2) |
INT16 |
-32767– +32767 |
Threshold drop-out value. The factory setting is 0. |
|
0x1A78 |
6777 |
– |
– |
– |
– |
– |
Reserved |
|
0x1A79 |
6778 |
R |
1 |
s |
INT16 |
0–3000 |
Drop-out time delay. The factory setting is 0. |
|
0x1A7A |
6779 |
R |
– |
– |
INT16U |
0–3 |
Operator: 0: ≥, 1: ≤, 2: =, 3: I ≥ I |
|
0x1A7B |
6780 |
R |
– |
– |
INT16U |
1–1919 |
|
|
0x1A7C |
6781 |
– |
– |
– |
– |
– |
Reserved |
|
(1) The value of the measurement identifier is the register number of the measurement. For example, the measurement identifier of current on phase 1 (I1) is 1016. (2) The unit of the threshold depends on the measurement identifier. For example, if the measurement identifier is I1, then the unit is A. |
|||||||
Predefined Alarms Codes
The following table describes the list of predefined alarms and corresponding codes from which the user can choose the 10 user-defined alarms and configure them with EcoStruxure Power Commission software.
|
Alarm Code |
Alarm Description |
|---|---|
|
1 (0x0000) |
Overcurrent instantaneous phase 1 |
|
2 (0x0001) |
Overcurrent instantaneous phase 2 |
|
3 (0x0002) |
Overcurrent instantaneous phase 3 |
|
4 (0x0003) |
Overcurrent instantaneous neutral |
|
5 (0x0004) |
Ground-fault current |
|
6 (0x0005) |
Undercurrent instantaneous phase 1 |
|
7 (0x0006) |
Undercurrent instantaneous phase 2 |
|
8 (0x0007) |
Undercurrent instantaneous phase 3 |
|
9 (0x0008) |
Overcurrent unbalance phase 1 |
|
10 (0x0009) |
Overcurrent unbalance phase 2 |
|
11 (0x000A) |
Overcurrent unbalance phase 3 |
|
12 (0x000B) |
Overvoltage (phase 1 to neutral) |
|
13 (0x000C) |
Overvoltage (phase 2 to neutral) |
|
14 (0x000D) |
Overvoltage (phase 3 to neutral) |
|
15 (0x000E) |
Undervoltage (phase 1 to neutral) |
|
16 (0x000F) |
Undervoltage (phase 2 to neutral) |
|
17 (0x0010) |
Undervoltage (phase 3 to neutral) |
|
18 (0x0011) |
Overvoltage unbalance (phase 1 to neutral) |
|
19 (0x0012) |
Overvoltage unbalance (phase 2 to neutral) |
|
20 (0x0013) |
Overvoltage unbalance (phase 3 to neutral) |
|
21 (0x0014) |
Over total apparent power |
|
22 (0x0015) |
Over total active power |
|
23 (0x0016) |
Over total active reverse power |
|
24 (0x0017) |
Over total reactive power |
|
25 (0x0018) |
Over total reactive reverse power |
|
26 (0x0019) |
Under total apparent power |
|
27 (0x001A) |
Under total active power |
|
28 (0x001B) |
Reserved |
|
29 (0x001C) |
Under total reactive power |
|
30 (0x001D) |
Reserved |
|
31 (0x001E) |
Leading power factor (IEEE) |
|
32 (0x001F) |
Reserved |
|
33 (0x001E) |
Leading or lagging power factor (IEC) |
|
34 (0x0021) |
Lagging power factor (IEEE) |
|
35 (0x0022) |
Over total harmonic distortion current phase 1 |
|
36 (0x0023) |
Over total harmonic distortion current phase 2 |
|
37 (0x0024) |
Over total harmonic distortion current phase 3 |
|
38 (0x0025) |
Over total harmonic distortion voltage (phase 1 to neutral) |
|
39 (0x0026) |
Over total harmonic distortion voltage (phase 2 to neutral) |
|
40 (0x0027) |
Over total harmonic distortion voltage (phase 3 to neutral) |
|
41 (0x0028) |
Over total harmonic distortion voltage (phase 1– 2) |
|
42 (0x0029) |
Over total harmonic distortion voltage (phase 2– 3) |
|
43 (0x002A) |
Over total harmonic distortion voltage (phase 3– 1) |
|
44–53 (0x002B–0x0034) |
Reserved |
|
54 (0x0035) |
Earth-leakage current |
|
55 (0x0036) |
Overcurrent (average) |
|
56 (0x0037) |
Over maximum current (I1, I2, I3, or neutral) |
|
57 (0x0038) |
Undercurrent instantaneous neutral |
|
58–59 (0x0039–0x003A) |
Reserved |
|
60 (0x003B) |
Undercurrent (average) |
|
61 (0x003C) |
Overcurrent demand phase 1 |
|
62 (0x003D) |
Overcurrent demand phase 2 |
|
63 (0x003E) |
Overcurrent demand phase 3 |
|
64 (0x003F) |
Overcurrent demand neutral |
|
65 (0x0040) |
Under minimum current (I1, I2, or I3) |
|
66 (0x0041) |
Undercurrent demand phase 1 |
|
67 (0x0042) |
Undercurrent demand phase 2 |
|
68 (0x0043) |
Undercurrent demand phase 3 |
|
69 (0x0044) |
Undercurrent demand neutral |
|
70 (0x0045) |
Over maximum current unbalance (I1, I2, or I3) |
|
71 (0x0046) |
Overvoltage (phase 1– 2) |
|
72 (0x0047) |
Overvoltage (phase 2– 3) |
|
73 (0x0048) |
Overvoltage (phase 3– 1) |
|
74 (0x0049) |
Reserved |
|
75 (0x004A) |
Overvoltage (average) |
|
76 (0x004B) |
Undervoltage (phase 1– 2) |
|
77 (0x004C) |
Undervoltage (phase 2– 3) |
|
78 (0x004D) |
Undervoltage (phase 3– 1) |
|
79 (0x004E) |
Over maximum voltage |
|
80 (0x004F) |
Undervoltage (average) |
|
81 (0x0050) |
Under minimum voltage |
|
82 (0x0051) |
Over maximum voltage unbalance (phases to neutral) |
|
83–85 (0x0052–0x0054) |
Reserved |
|
86 (0x0055) |
Overvoltage unbalance (phase 1– 2) |
|
87 (0x0056) |
Overvoltage unbalance (phase 2– 3) |
|
88 (0x0057) |
Overvoltage unbalance (phase 3– 1) |
|
89 (0x0058) |
Over maximum voltage unbalance |
|
90 (0x0059) |
Phase sequence |
|
91 (0x005A) |
Reserved |
|
92 (0x005B) |
Under frequency |
|
93 (0x005C) |
Over frequency |
|
94–98 (0x005D–0x0061) |
Reserved |
|
99 (0x0062) |
Over active power demand |
|
100–120 (0x0063–0x0077) |
Reserved |
|
121 (0x0078) |
Leading cosϕ (IEEE) |
|
122 (0x0079) |
Reserved |
|
123 (0x007A) |
Leading or lagging cosϕ (IEC) |
|
124 (0x007B) |
Lagging cosϕ (IEEE) |
|
125 (0x007C) |
Overcurrent thermal image motor |
|
126 (0x007D) |
Undercurrent thermal image motor |
|
127–140 (0x007E–0x008B) |
Reserved |
|
141 (0x008C) |
Overcurrent maximum demand phase 1 |
|
142 (0x008D) |
Overcurrent maximum demand phase 2 |
|
143 (0x008E) |
Overcurrent maximum demand phase 3 |
|
144 (0x008F) |
Overcurrent maximum demand neutral |
|
145 (0x0090) |
Lead |
|
146 (0x0091) |
Lag |
|
147 (0x0092) |
Quadrant 1 |
|
148 (0x0093) |
Quadrant 2 |
|
149 (0x0094) |
Quadrant 3 |
|
150 (0x0095) |
Quadrant 4 |
|
151–255 (0x0096–0x00FE) |
Reserved |
|
256 (0x00FF) |
Contact wear |