DOCA0213EN-03

List of MicroLogic Trip Unit Commands and Error Codes

List of Commands

The following table lists the available MicroLogic trip unit commands, their corresponding command codes and user profiles. Follow the command execution procedures.

Command

Command code

User profile

Long-time protection

45192

Administrator

Short-time protection

45193

Administrator

Instantaneous protection

45194

Administrator

Ground-fault protection

45195

Administrator

Earth-leakage protection

45196

Administrator

Neutral protection

45197

Administrator

Jam protection

45448

Administrator

Underload protection

45449

Administrator

Unbalance protection

45450

Administrator

Long-start protection

45451

Administrator

Acknowledge a latched output

46216

Administrator or Operator

Acknowledge a trip

46217

Administrator

Set up ENVT presence

46472

Administrator

Reset minimum/maximum

46728

Administrator or Operator

Start/stop synchronization

46729

Administrator or Operator

Power flow sign configuration

47240

Administrator

Power factor sign configuration

47241

Administrator

Energy accumulation mode configuration

47242

Administrator

Current demand configuration

47243

Administrator

Power demand configuration

47244

Administrator

Set up nominal voltage Vn display

47245

Administrator

Phase rotation

47246

Administrator

Error Codes

Error codes generated by MicroLogic trip units are the generic error codesResult of the Command.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?