DOCA0213EN-03

Modbus Network Parameters

Modbus Locking Status

Address

Register

RW

Unit

Type

Range

Description

0x2E72

11891

R

INT16U

1–3

Modbus locking pad position

  • 1 = Modbus locking pad is on the locked position

  • 3 = Modbus locking pad is on the open position

Validity Duration of Data

Address

Register

RW

Unit

Type

Range

Description

0x306A

12395

R

s

INT16U

5–300 (in steps of 5 s)

Duration of validity of data in the dataset

Auto-Speed Sensing State

Address

Register

RW

Unit

Type

Range

Description

0x306E

12399

R

INT16U

0–1

Auto-Speed sensing state

  • 0 = Auto-Speed sensing is disabled

  • 1 = Auto-Speed sensing is enabled (factory setting)

Communication Interface Modbus Address

Address

Register

RW

Unit

Type

Range

Description

0x306F

12400

R

INT16U

1–99

Communication interface Modbus address

Modbus Parity

Address

Register

RW

Unit

Type

Range

Description

0x3070

12401

R

INT16U

1–3

Modbus parity

  • 1 = no parity (none)

  • 2 = even parity (factory setting)

  • 3 = odd parity

Modbus Baud Rate

Address

Register

RW

Unit

Type

Range

Description

0x3071

12402

R

INT16U

5–8

Modbus Baud rate

  • 5 = 4800 Baud

  • 6 = 9600 Baud

  • 7 = 19200 Baud (factory setting)

  • 8 = 38400 Baud

Number of Stop Bits

Address

Register

RW

Unit

Type

Range

Description

0x3072

12403

R

INT16U

0–5

Number of stop bits

  • 0 = no change

  • 1 = standard Modbus

  • 2 = 1/2 stop bit

  • 3 = 1 stop bit

  • 4 = 1 and 1/2 stop bit

  • 5 = 2 stop bits

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?