DOCA0213EN-03

List of IFE/EIFE Interface Commands

List of Commands for IFE/EIFE Interfaces

The following table lists the IFE/EIFE interface commands, their corresponding command codes and user profiles. Follow the command execution procedures accordingly.

Command

Command code

User profile

Get current time

768

No password required

Set absolute time

769

No password required

Write user application name

1032

No password required

Set validity duration of the data

41868

Administrator, Services, Engineer, or Operator

List of Specific Commands for EIFE Interface

The following table lists the EIFE interface commands, their corresponding command codes and user profiles. Follow the command execution procedures.

Command

Command code

User profile

Reset EIFE alarms

41099

Administrator or Operator

Preset cradle/drawer counters

41352

Administrator or Operator

Preset regrease timers

41353

Administrator or Operator

Get events

50560

No password required

Error Codes

Error codes generated by the IFE/EIFE interface are the generic error codes Result of the Command.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?