DOCA0213EN-03

Status

Alarms Status

The alarms status register indicates the current status of the alarms:

  • Alarm bit = 0: Alarm is not active.

  • Alarm bit = 1: Alarm is active.

The following table describes the values for each bit of the alarm status register:

Address

Register

RW

X

Unit

Type

Range

Bit

Description

0x1647

5704

R

INT16U

Alarm status

0

User-defined alarm 201

1

User-defined alarm 202

2

User-defined alarm 203

3

User-defined alarm 204

4

User-defined alarm 205

5

User-defined alarm 206

6

User-defined alarm 207

7

User-defined alarm 208

8

User-defined alarm 209

9

User-defined alarm 210

10

Long-time protection Ir pre-alarm (PAL Ir)

11

Earth-leakage protection IΔn pre-alarm (PAL IΔn)

12

Ground-fault protection Ig pre-alarm (PAL Ig)

13–15

Reserved

SDx Module Status

The SDx module status register indicates the status and the validity of the SDx outputs (2 outputs maximum):

  • Status bit = 0: The output is open.

  • Status bit = 1: The output is closed.

  • Validity bit = 0: The output status is unknown.

  • Validity bit = 1: The output status is known.

The following table describes the values for each bit of the SDx module status register:

Address

Register

RW

X

Unit

Type

Range

Bit

Description

0x2298

8857

R

INT16U

SDx module status

0

Status of output 1

1

Status of output 2

2–7

Reserved

8

Validity of output 1

9

Validity of output 2

10–15

Reserved

Trip Status

The trip status register indicates the current status of the trip:

  • Trip bit = 0: Trip is not active.

  • Trip bit = 1: Trip is active.

The following table describes the values for each bit of the trip status register:

Address

Register

RW

X

Unit

Type

Range

Bit

Description

0x270F

10000

R

INT16U

Trip status

0

Long-time protection Ir

1

Short-time protection Isd

2

Instantaneous protection Ii

3

Ground-fault protection Ig

4

Earth-leakage protection IΔn

5

Integrated instantaneous protection

6

Trip unit internal failure (STOP)

7

Instantaneous with earth-leakage protection

8

Unbalance motor protection Iunbal

9

Jam motor protection Ijam

10

Underload motor protection Iunderload

11

Long-start motor protection Ilongstart

12

Reflex tripping protection

13–15

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?