DOCA0213EN-03

Communication Test

The user can test the communication between all the ULP modules connected to the BSCM Modbus SL/ULP module. There is no physical button. Connect to EcoStruxure Power Commission software and click the Locate button to launch the communication test between all the ULP modules connected to the BSCM Modbus SL/ULP module for 15 seconds.

During the test, all the ULP modules keep working normally.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?