DOCA0213EN-03

Hardware Description

Description

A Ethernet 1 and Ethernet 2 RJ45 communication ports

B 24 Vdc power supply terminal block

C QR code to product information

D Ethernet communication LEDs

E Module status LED

F Network status LED

G Sealable transparent cover

H Reset button

I ULP status LED

J Test button (accessible even with closed cover)

K Locking pad

L Modbus traffic status LED (IFE server only)

M Device name label

N Two RJ45 ULP ports

O Grounding connection

For information on installation, consult the instruction sheet available on the Schneider Electric website: QGH13473.

Mounting

The IFE communication interface mounts on a DIN rail. The stacking accessory enables the connection of several IFM communication interfaces to an IFE server without additional wiring.

NOTE: The stacking feature is available only for the IFE server with the part number LV434002.

24 Vdc Power Supply

The IFE communication interface must always be supplied with 24 Vdc. The power to the IFM communication interfaces stacked to an IFE server are supplied by the IFE server and it is not necessary to supply power to them separately.

It is recommended to use a UL listed and recognized limited voltage/limited current or a class 2 power supply with a 24 Vdc, 3 A maximum.

NOTE: For 24 Vdc power supply connection, use copper conductors only.

Ethernet Communication LEDs

The Ethernet communication dual color LEDs, indicate the status of the Ethernet ports ETH1 and ETH2.

LED Indication

Status Description

OFF

No power or no link

Steady yellow

10 Mbps, link established, and no activity

Blinking yellow

10 Mbps, ongoing activity

Steady green

100 Mbps, link established, and no activity

Blinking green

100 Mbps, ongoing activity

Module Status LED

The module status dual color LED indicates the IFE communication interface status.

LED Indication

Status Description

Action

OFF

No power

None

Steady green

IFE communication interface operational

None

Blinking green (250 ms ON, 250 ms OFF)

Hidden control webpage available

None

Blinking green (500 ms ON, 500 ms OFF)

IFE communication interface firmware corrupted

Contact your local Schneider Electric service team for support.

Blinking red (500 ms ON, 500 ms OFF)

IFE communication interface in degraded mode

Replace ULP module at the next maintenance operation.

Steady red

IFE communication interface out of service

None

Blinking green/red (1 s green, 1 s red)

Firmware update in progress

None

Blinking green/red (250 ms green, 250 ms red)

Self-test in progress

None

Network Status LED

The network status dual color LED, indicates the Ethernet network status.

LED Indication

Status Description

OFF

No power or no IP address

Steady green

Valid IP address

Steady red

Duplicated IP address

Blinking green/red (250 ms green, 250 ms red)

Self-test in progress

Steady amber

Error in IP configuration

Modbus Serial Line Traffic LED

The Modbus serial line traffic yellow LED, indicates that the traffic is being transmitted or received over the Modbus serial line network through the IFE server.

The LED is ON during the transmission and reception of the messages. The LED is OFF otherwise.

NOTE: The LED is OFF on the IFE communication interface (part number LV434001).

Modbus Address

The IFE communication interface accepts the Modbus address of the IMU to which it is connected.

The Modbus address is 255 and cannot be changed.

Locking Pad

The locking pad on the front panel of the IFE communication interface enables or disables the ability to send the remote control commands over the Ethernet network to the IFE communication interface, and to the other modules of the IMU.

  • If the arrow points to the open padlock (factory setting), remote control commands are enabled.

  • If the arrow points to the closed padlock, remote control commands are disabled.

    The only remote control command that is enabled even if the arrow points to the closed padlock, is the set absolute time command.

Test Button

The test button has two functions, according to the duration of the button pressed.

Time Range

Function

1–5 s

Tests the connection between all the ULP modules for 15 s.

10–15 s

Activates the hidden configuration mode.

NOTE: The hidden configuration is not activated if the button is pressed for more than 15 s.

Reset Button

When the reset button is pressed for 1–5 s, it forces the IP acquisition mode to the factory default setting (DHCP).

ULP Status LED

The yellow ULP status LED describes the mode of the ULP module.

ULP LED

Mode

Action

Nominal

None

Conflict

Remove extra ULP module

Degraded

Replace ULP module at the next maintenance operation

Test

None

Non-critical firmware discrepancy

Use EcoStruxure Power Commission software to check the firmware and hardware compatibility and follow the recommended actions

Non-critical hardware discrepancy

Configuration discrepancy

Install missing features

Critical firmware discrepancy

Use EcoStruxure Power Commission software to check the firmware and hardware compatibility and follow the recommended actions

Critical hardware discrepancy

Stop

Replace ULP module

Power OFF

Check power supply

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?