DOCA0213EN-03

Maintenance Indicators

General Description

The BSCM module has 7 counters that help to manage the ComPacT NSX circuit breaker.

The BSCM module counters have the following properties:

  • All the counters are saved in non-volatile memory to prevent data loss in case of power loss.

  • The cumulating OF counter is read only. It stops incrementing when it reaches the maximum value 4 294 967 295.

  • The user can preset all counters (except the cumulating OF counter) to any value from 0 to 65535. The counters stop incrementing when they reach the maximum value 65535.

  • Tthe OF counter and close circuit breaker command counter have a threshold which can be set by the user, to any value from 0 to 65534.

    The factory setting is 5000. An alarm is generated when a counter reaches the threshold.

BSCM Module Counters

Address

Register

RW

X

Unit

Type

Range

Description

0x023A–

0x023B

571–

572

R

1

INT32U

0–4 294 967 295

Cumulating OF counter (non-resettable open to close counter)

0x023C

573

R-WC

1

INT16U

0–65535

OF counter (resettable open to close counter)

0x023D

574

R-WC

1

INT16U

0–65535

SD counter (Close to SD position)

0x023E

575

R-WC

1

INT16U

0–65535

SDE counter (Close to SDE position)

0x023F

576

R-WC

1

INT16U

0–65535

Open circuit breaker command counter

0x0240

577

R-WC

1

INT16U

0–65535

Close circuit breaker command counter

0x0241

578

R-WC

1

INT16U

0–65535

Reset circuit breaker command counter

0x0242–0x0243

579–580

Reserved

0x0244

581

R-WC

1

INT16U

0–65535

OF counter threshold

The factory setting is 5000.

0x0245

582

R-WC

1

INT16U

0–65535

Close circuit breaker command counter threshold

The factory setting is 5000.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?