DOCA0213EN-03

Communication Test

To test the serial line communication on the various circuit breakers, it is recommended to use EcoStruxure Power Commission software.

If a PC running EcoStruxure Power Commission (EPC) software and connected on the Modbus network is able to read data from the IMU, the communication is established. Refer to the EcoStruxure Power Commission Online Help.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?