DOCA0213EN-03

Configuration of the SDx Module

Output 1

A read request of 3 registers is necessary to read the output 1 parameters.

The user can check the status and the validity of output 1 at register 8857.

Address

Register

RW

X

Unit

Type

Range

Description

0x2648

9801

R

1

INT16U

0–4

Output mode

0 = normal mode

1 = latched mode

2 = time delayed mode

3 = closed forced mode

4 = open forced mode

0x2649

9802

R

1

s

INT16U

1–360

Delay (if the output mode is set to 2).

The factory setting is 1 s.

0x264A

9803

R

1

INT16U

0–65535

Alarm identifier (201–210, 1013, 1014, 1015).

The alarm identifier is set to 0 if there is no alarm.

Output 2

A read request of 3 registers is necessary to read the output 2 parameters.

The user can check the status and the validity of output 2 at register 8857.

Address

Register

RW

X

Unit

Type

Range

Description

0x264F

9808

R

1

INT16U

0–4

Output mode

0 = normal mode

1 = latched mode

2 = time delayed mode

3 = closed forced mode

4 = open forced mode

0x2650

9809

R

1

s

INT16U

1–360

Delay (if the output mode is set to 2).

The factory setting is 1 s.

0x2651

9810

R

1

INT16U

0–65535

Alarm identifier (201–210, 1013, 1014, 1015).

The alarm identifier is set to 0 if there is no alarm.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?