DOCA0213EN-03

BSCM Modbus SL/ULP Module Identification

Product Identification

Address

Register

RW

X

Unit

Type

Range

Description

0x4CD1

19666

R

INT16U

15149

Product identification = 15149 for the BSCM Modbus SL/ULP module

BSCM Modbus SL/ULP Module Identifier

The BSCM Modbus SL/ULP module serial number is composed of a maximum of 15 alphanumeric characters with the following format: PPYYWWDLLLNNNNN.

  • PP = plant code

  • YY = year of fabrication (05–99)

  • WW = week of fabrication (01–53)

  • D = day of fabrication (1–7)

  • LLL = unique final assembly manufacturing line number or machine number within the plant (A–Z or 0–9).

  • NNNNN= unique product number generated on the day of manufacture by the plant manufacturing line or the plant machine (00001–99999).

A read request of eight registers is necessary to read the BSCM Modbus SL/ULP module serial number.

Address

Register

RW

X

Unit

Type

Range

Description

0x4CC8

19657

R

OCTET STRING

‘PP’

0x4CC9

19658

R

OCTET STRING

05–99

‘YY’

0x4CCA

19659

R

OCTET STRING

01–53

‘WW’

0x4CCB

19660

R

OCTET STRING

1–7

‘D’

0x4CCC

19661

R

OCTET STRING

A–Z, 0–9

‘LLL’

0x4CCD

19662

R

OCTET STRING

00–99

‘NN’

0x4CCE

19663

R

OCTET STRING

01–99

‘NN’

0x4CCF

19664

R

OCTET STRING

01–99

‘N’ (the NULL character ends the serial number)

BSCM Modbus SL/ULP Module Identification (Both Modbus and ULP Architecture)

The following table is valid for the three modes of the BSCM Modbus SL/ULP module:

  • Modbus SL only mode

  • ULP only mode

  • Modbus SL and ULP mode

Address

Register

RW

Unit

Type

Range

Description

0x4C2B–0x4C34

19500–19509

R-WC

OCTET STRING

User application name = ComPacT NSX (by default)

0x4C35–0x4C4A

19510–19531

Reserved

0x4C4B–0x4C8A

19532–19595

R

OCTET STRING

Vendor URL = https://www.se.com/

0x4C8B–0x4C9A

19596–19611

R

OCTET STRING

Product family = Gateway and server

0x4C9B–0x4CA2

19612–19619

R

OCTET STRING

Product range = ComPacT NSX

0x4CA3–0x4CAA

19620–19627

R

OCTET STRING

Product model = BSCM Modbus SL/ULP

0x4CAB–0x4CB2

19628–19635

R

OCTET STRING

Firmware revision

0x4CB3–0x4CBC

19636–19645

R

OCTET STRING

Vendor name = Schneider Electric

0x4CBD–0x4CC6

19646–19655

R

OCTET STRING

Product code = LV434220

0x4CC7–0x4CD0

19656–19665

R

OCTET STRING

Serial number

0x4CD1

19666

R

INT16U

Product identifier = 15149 for BSCM Modbus SL/ULP

0x4CD2–0x4CDB

19667–19676

R

OCTET STRING

Hardware revision

0x4CDC–0x4CE5

19677–19686

R-WC

OCTET STRING

Product capability = Other (by default)

0x4CE6–0x4CF5

19687–19702

R-WC

OCTET STRING

Product user tag = My tags (by default)

BSCM Modbus SL/ULP Module Identification (Only Modbus Architecture)

The following table is valid for the two following modes:

  • Modbus SL only mode.

  • Modbus SL and ULP mode

Address

Register

RW

Unit

Type

Range

Description

0x2800–0x2809

10241–10250

R-WC

OCTET STRING

User application name = ComPacT NSX (by default)

0x280A–0x281F

10251–10272

Reserved

0x2D9D–0x2DDC

11678–11741

R

OCTET STRING

Vendor URL = https://www.se.com/

0x2DDE–0x2DED

11743–11758

R

OCTET STRING

Product family = Gateway and server

0x2DEE–0x2DF5

11759–11766

R

OCTET STRING

Product range = ComPacT NSX

0x2DF6–0x2DFD

11767–11774

R

OCTET STRING

Product model = BSCM Modbus SL/ULP

0x2DFE–0x2E05

11775–11782

R

OCTET STRING

Firmware revision

0x2E2E–0x2E37

11823–11832

R

OCTET STRING

Vendor name = Schneider Electric

0x2E38–0x2E41

11833–11842

R

OCTET STRING

Product code = LV434220

0x2E5B–0x2E64

11868–11877

R

OCTET STRING

Serial number

0x2E7B

11900

R

INT16U

Product identifier = 15149 for BSCM Modbus SL/ULP

0x2E90–0x2E99

11921–11930

R

OCTET STRING

Hardware revision

Read Device Identification

The Read Device Identification function is used to access in a standardized manner the information required to identify a device. The description is made up of a set of objects (ASCII character strings).

A complete description of the Read Device Identification function is available at www.modbus.org.

The coding for the identification of the BSCM Modbus SL/ULP module is the following:

Name

Type

Description

Vendor name

OCTET STRING

‘Schneider Electric’ (18 characters)

Product code

OCTET STRING

LV434220

Firmware revision

OCTET STRING

‘XXX.YYY.ZZZ’

Vendor URL

OCTET STRING

‘www.se.com’

Product name

OCTET STRING

BSCM Modbus SL/ULP (LV434220)

Model name

OCTET STRING

Communication module

User application name

OCTET STRING

ComPacT NSX (by default)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?