Date Management
Introduction
Each module of the IMU uses its date to time-stamp events and history registers.
The date of the IMU modules is updated in two steps:
-
External synchronization: The Modbus client synchronizes the IFM or IFE communication interface, or the BSCM Modbus SL/ULP module in Modbus SL only mode and in Modbus SL and ULP mode.
-
Internal synchronization:
-
If the BSCM Modbus SL/ULP module is in ULP only mode, the IFM or IFE communication interface synchronizes all ULP modules connected in the IMU, including the BSCM Modbus SL/ULP module.
-
If the BSCM Modbus SL/ULP module is in Modbus SL only mode or in Modbus SL and ULP mode, the BSCM Modbus SL/ULP module synchronizes all ULP modules connected in the IMU.
-
External Synchronization
There are three ways to externally synchronize the IFM or IFE communication interface or the BSCM Modbus SL/ULP module in Modbus SL only mode or in Modbus SL and ULP mode:
-
Manually with EcoStruxure Power Commission software.
-
By programming of the Modbus client using:
-
Either the Modbus function set date and time: Function code 43-16 Write Functions.
-
Or the set absolute time command through the IFM or IFE communication interface, or through the BSCM Modbus SL/ULP module.
-
-
Automatically:
-
With IFE communication interface configured as SNTP mode.
-
The communication interface is considered as externally synchronized if the last synchronization has occurred within the last 2 hours.
Internal Synchronization
The date and time is received from:
-
The IFM communication interface
-
Or the IFE communication interface
-
Or the BSCM Modbus SL/ULP module, in Modbus SL only mode or Modbus SL and ULP mode