DOCA0187EN-03

Front Face Description

Front Face with Direct Rotary Handle

The circuit breaker operating controls, operation indicators, settings, and locking mechanisms for the direct rotary handle are on the front of the circuit breaker.

There are two models of rotary handle:

  • Black handle for standard applications

  • Red handle on yellow bezel for machine control applications

A Faceplate

B Direct rotary handle for opening, closing, and resetting

C Push-to-trip button

D Trip unit

E Trip unit adjustment dials

For more information about rotary handle configuration and installation, consult the instruction sheets on the Schneider Electric website:

  • NNZ4765907, Direct mounted rotary handle for ComPacT NSX100-250

  • NNZ4766407, Direct mounted rotary handle for ComPacT NSX400-630

Front Face with Extended Rotary Handle

For circuit breakers with an extended rotary handle:

  • The circuit breaker operating controls are on the door escutcheon.

  • The operation indicators and settings are only accessible when the door is open

  • The locking mechanisms are on the circuit breaker (optional) and on the door escutcheon (door closed).

There are two models of extended rotary handle:

  • Black handle for standard applications

  • Red handle on yellow bezel for machine control applications

Cabinet door open Cabinet door closed

A Faceplate

B Open door shaft operator

C Push-to-trip button

D Trip unit

E Trip unit adjustment dials

F Extended rotary handle for opening, closing, and resetting

For more information about extended rotary handle installation, consult the instruction sheets on the Schneider Electric website:

  • NNZ4766007, Extended rotary handle for ComPacT NSX100-250

  • NNZ4766507, Extended rotary handle for ComPacT NSX400-630

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.